Digital output energy pulsing
You can configure a device’s built-in digital outputs for energy pulsing applications. When a digital output is configured for energy pulsing, the device sends a readable pulse based on the measured energy source value. This pulse can be used as an input to another energy monitoring system.