Configuring digital output energy pulsing
You can configure your device’s built-in digital outputs for energy pulsing.
When you configure your device, all possible ports may be listed, regardless of what is physically available on your device.
Ensure that the digital output port is available for energy pulsing and not associated with another function.
Prerequisites:
- Open the device table of contents.
- Connect to your device.
- Pulse weight calculations. For more information on how to calculate Kt, see Calculating the pulse weight (Kt).
To configure digital output energy pulsing:
- Select > .
- Go to the energy pulsing source that you want to configure.
- Enter your Digital output energy pulsing settings.
- Select Save Working Copy.
- Synchronize changes.