LED energy pulsing settings
LED energy pulsing settings
Parameter | Values | Description |
---|---|---|
Source | Linked register | The measured value that you want to pulse the LED when Kt is reached. Source must be in units of kW. |
Enable | Linked register |
Linking this parameter enables or disables LED pulsing depending on the state of the linked register. Linking Enable is optional. LED energy pulsing is enabled by default when Enable is unlinked. Note: Configuring this setting should only be performed by users with advanced knowledge of ION, the device template, and the power system the device is connected to. |
Int Mode | Net, Forward, Reverse, Absolute |
Sets the integration mode:
|
Kt | 0.01–1000000000 |
Specifies how many energy units in Wh, VARh or VAh are accumulated before pulsing the LED (pulse weight). For example, for Wh Del, Kt would be the amount of real energy delivered (Wh Del) per pulse. For more information on how to calculate Kt, see Calculating the pulse weight (Kt). |
Pulse Width | 0.01–1.0 |
The minimum time (in seconds) between LED pulse transitions. |
Pulser Mode | Always, Test Only |
Sets the energy pulsing LED behavior:
|
Pulse Overload | Read-only |
Feedback on the state of the LED configured for energy pulsing. Pulse Overload has three states:
|