LED energy pulsing

Use LED energy pulsing to configure your device’s energy pulsing LEDs. When the device LEDs are configured, the device sends a signal to the built-in energy pulsing LEDs based on the measured energy source value. These LED pulses can be used for accuracy verification.