Clean Installation of Database

This page of the Installation Wizard is only displayed when you install Geo SCADA Expert for the first time on a machine.

When you install Geo SCADA Expert for the first time on a machine, the server will start in demonstration mode as no license has been attached yet.

If you have a license for the server, or if you intend to use the example projects, you can move directly to the next page of the Installation Wizard. To do this, ensure that the Enable 100-Point Indefinite Demo License check box is clear, and click Next. Refer to Server License Settings - Geo SCADA Expert for more information on how you can add a license file for the server.

If you do not have a license for the server, you can use the Geo SCADA Expert Installer's Clean Installation of Database window to select the type of demonstration license that you want to use.

There are two types of demonstration licenses that you can opt for: