Geo SCADA Expert Server Requirements
In the following sections, we describe the recommended specifications for servers that are to run Geo SCADA Expert:
- Servers and Desktop Computers
- Disk Drives and RAID Arrays
- Virtualization and Cloud
- Operational Limitations - Geo SCADA Expert Server
- Recommended Geo SCADA Expert Server Configurations.
You should also refer to the following sections, which apply to both Geo SCADA Expert servers and Geo SCADA Expert clients:
- Operating Systems
- Screen Resolution and Color Depth
- Geo SCADA Expert Prerequisite Components
- File Locations (Default)
- Certificates for Geo SCADA Expert Server and Client Connections
- Web Browser Support .
Virtual ViewX is supported by Geo SCADA Expert 2019 onwards. We strongly recommend that you install the Virtual ViewX server on a different machine to the Geo SCADA Expert server. This is to avoid potential performance issues due to the number of resources that each application uses.
If you do install Geo SCADA Expert and Virtual ViewX on the same machine, both applications must have the same version and build number. This is because the applications share some resources.