Display Events

Associated with: Any item in the database

Security permission required to access this option: Read

Select this option on the Object Menu to display an Events List (see Events).

Select this option from an individual database item to display an Events List that only includes events for that particular item.

Select this option from a Group, Group Instance, or Group Template to display an Events List that only includes events for the items in that Group, Group Instance, or Group Template (including items in any subgroups).

Events Lists are pre-filtered by time—the period for which events are initially shown is defined by the Event List Range specified for your user account (or the Guest or Web user account if you are not logged onto the system). Your user account and security permissions might further restrict the entries in the Events List to those that are likely to be of interest to you.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.