Actions Associated with Slave Outstations on Advanced Drivers

With most advanced driver setups, Geo SCADA Expert is the SCADA master. Some drivers support slave functionality, whereby the Geo SCADA Expert system acts as an outstation or similar device and reports any data changes back to its SCADA master (see Master-Slave Communications). On systems on which Geo SCADA Expert is a slave, the Slave outstations support a combination of these actions:

Further Information

‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.

For information on any slave outstation-specific actions that are not listed above, see the relevant driver guide.