Errors When Create Points Last Ran

Associated with: Sparkplug™ Edge Nodes and Sparkplug Devices

This status attribute indicates whether Geo SCADA Expert detected any issues when the Create Points from Birth Metrics pick action was last executed on the selected Sparkplug Edge Node or Sparkplug Device.

A value of 0 (zero) indicates that the point creation process that was last triggered by the Create Points from Birth Metrics pick action completed successfully.

If a value other than 0 is displayed, check the time and date that has been reported by the Point Configuration Error Alarm, and then look at the entries in the Alarms List and Events List from that time onwards to ascertain the issues that occurred. The entries will be assigned the Sparkplug Object Creation Error category (see Alarm and Event Categories that are Specific to the Sparkplug™ Driver).