Introduction to the NTP Monitor Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

  • Install and run the driver
  • Ensure that the driver is licensed
  • Configure the required database items and settings on the driver
  • Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.

Intended Audience

This guide is designed for use by engineers who are responsible for configuring NTP-related settings. It can also be used by system administrators who can use the NTP driver’s diagnostic features for fault finding.

Document Scope

This guide explains how to configure Geo SCADA Expert’s NTP Driver to monitor a Network Time Protocol (NTP) server. It also provides information on NTP stratum ranking and the NTP driver’s diagnostic features.

The Network Time Protocol (NTP) is an Internet protocol that is used for synchronizing the system clocks on computer systems. The Geo SCADA Expert NTP Monitor Driver monitors the accuracy of such synchronization.

We recommend that you run NTP, or an equivalent time synchronization mechanism, on your Geo SCADA Expert system. This will synchronize the system clocks of the computers on your system.

If required, on systems that are running NTP, you can also run the Geo SCADA Expert NTP Monitor Driver and configure NTP Monitor items in the database to enable you to assess the accuracy with which those system clocks are being synchronized.

This Guide to the NTP Monitor Driver explains:

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

On the Modules tab of the Geo SCADA Expert Server Status Tool, this particular driver is listed as the NTP driver. The logging options that are available to the driver are common to many simple drivers—for information, see Driver Log File Options that are Common to Many Simple Drivers in the Geo SCADA Expert Guide to Simple Drivers.

You can achieve high accuracy time (such as synchronizing time to within an accuracy of 1ms) using W32Time, providing that certain criteria are satisfied. For more information, see https://learn.microsoft.com/en-us/windows-server/networking/windows-time-service/support-boundary. However, if you choose to use another third-party NTP client to maintain accurate time, remember to disable Windows Time (W32Time).

For information on running NTP (as oppose to the NTP Monitor driver) and on synchronizing system clocks using NTP, see the NTP website (http://www.ntp.org).

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).