Configure Geo SCADA Expert to Communicate with Downstream Server/Remote Devices
You can configure Geo SCADA Expert to communicate with SCADAPack x70 devices that themselves provide access to other server/remote devices that are further downstream in your operational network. If Geo SCADA Expert is to communicate with those downstream devices via the SCADAPack x70 devices, in addition to the usual SCADAPack x70 configuration, you have to:
- Configure a SCADAPack x70 DNP3 Remote Device per downstream DNP3 remote device
- Configure a SCADAPack x70 Modbus Server Device per downstream Modbus Server device. For each of these, configure a SCADAPack x70 Modbus Point Scanner for each block of registers to read/write. For more information, see Configure a Modbus Server Device and see Configure a Modbus Point Scanner.
- Configure the relevant settings on the Mapping tab of each SCADAPack x70 Analog, Digital, or Counter Configuration item that represents an input or output on each downstream device (see Configure the Properties on the Mapping Tab). (SCADAPack x70 String Configuration items are not supported on downstream devices.)
We recommend that you use status points to monitor the status of, and control points to control, the downstream server/remote devices. These points comprise internal points that are built into the SCADAPack x70 devices. To make use of these points, in the database you have to:
- Create and configure a SCADAPack x70 Configuration item of the relevant type (analog or digital) for each status/control item that you want to use.
- Create and configure a protocol-specific SCADAPack x70 Point of the relevant type (analog, digital or binary) to associate with the above Configuration items, in order to monitor the status data in Geo SCADA Expert.
- Associate each SCADAPack x70 Configuration item with the relevant status/control item that you want to monitor or control. (depending on the protocol used, see Configure Modbus Server Device Status and Control Object Associations, or for DNP3 see Configure Object Associations for a Remote Device.)
For example, to monitor the communications status of a downstream server/remote device, use the Communication Status field on the SCADAPack x70 Server/Remote Device to associate that server/remote device with the relevant status point.
Likewise, to control whether a downstream server/remote device is in service, use the Put Device In Service field on the SCADAPack x70 Server/Remote Device to associate that server/remote device with the relevant control point.
The protocol that you use for the status points and downstream server/remote devices must correspond to the communications protocol that the SCADAPack x70 devices use to communicate with the downstream server/remote devices. That protocol might well differ to the communications protocol that Geo SCADA Expert uses to communicate with the SCADAPack x70 devices themselves.