Configure the Properties on the Mapping Tab

The Forms of SCADAPack x70 <Point Type> Configuration items include a Mapping tab. By default, the settings on this tab are disabled (the Mapping property is set to 'No Mapping').

You only need to set the 'Mapping' property to another option if one of the following applies:

Either:

  • The SCADAPack x70 device with which the SCADAPack x70 Configuration item is associated requests data from a Server/Remote device

and:

  • The SCADAPack x70 Configuration item that you are configuring represents an input or output on that Server/Remote device.

    If both of the above apply, use the Mapping property to specify the communications protocol that the SCADAPack x70 device is to use to communicate with the Server/Remote device. Other properties will become available on the Mapping tab; use the properties to specify the required settings to enable the SCADAPack x70 device to retrieve the data from the Server/Remote device.

    If you want to use the data from the Server/Remote device in Geo SCADA Expert, in addition to configuring the relevant settings on the Mapping tab, you have to associate the SCADAPack x70 Configuration item with a SCADAPack x70 protocol-specific Point. You use the Point to specify how Geo SCADA Expert processes the data that it retrieves from the Server/Remote device for that particular input or output (see Points and Configuration Items Supported by the Driver).

Or:

  • The SCADAPack x70 <Point Type> Configuration item is being used to monitor or control system data on a SCADAPack x70 device.

    In which case, use the Mapping property to specify the item of system data with which the SCADAPack x70 Configuration item is associated.

    If you want to use the SCADAPack x70 device's system data in Geo SCADA Expert, in addition to configuring the relevant settings on the Mapping tab, you need to associate the SCADAPack x70 Configuration item with a SCADAPack x70 protocol-specific Point. You use the Point to specify how Geo SCADA Expert processes the system data that it retrieves from the SCADAPack x70 device for that particular input or output (see Points and Configuration Items Supported by the Driver).

Further Information

Specify the role of a SCADAPack x70 device in a SCADA network: see Configure the Device Options.

Configure Geo SCADA Expert to Communicate with Downstream Server/Remote Devices.

Use system data to trigger Daylight Saving Time (DST) adjustments: see Configure the Time Zone Settings for Local Operations.