Create Points Status
Associated with: SCADAPack x70 Device Configuration items
The Create Point Status attribute is only displayed if the Create Protocol Points pick action has ever been executed on the selected SCADAPack x70 Device Configuration item.
When the Create Protocol Points pick action is triggered, the status attribute might initially show the following value until Geo SCADA Expert starts to execute the pick action:
Transaction: Queued
While the Create Protocol Points pick action is in progress, the status attributes provides information about the progress of that action.
Transaction: In Progress; Progress: 57.70% completed
Once the Create Protocol Points action has completed executing, the status attribute displays the following value:
Transaction: Idle
Use the status attribute in conjunction with the Create Points Summary status attribute.
Further Information