Create Points Summary
Associated with: SCADAPack x70 Device Configuration items
The Create Points Summary status attribute is only displayed if the Create Protocol Points pick action has ever been executed on the selected SCADAPack x70 Device Configuration item.
While the Create Protocol Points pick action is in progress, the status attribute provides information about the progress of that action.
SCADAPack x70 create DNP3 points transaction queued at 2025-05-29 10:05:32, progressing...
Once the Create Protocol Points action has completed executing, the status attribute provides information about the action's completion date and time. It also indicates the number of SCADAPack x70 protocol-specific Points that Geo SCADA Expert has created as a result of the pick action being executed.
SCADAPack x70 create DNP3 points transaction queued at 2025-05-29 10:05:32 completed - 1000 points created
For information about what activities you should perform once the action has completed executing, see Create Protocol Points.
Use the status attribute in conjunction with the Create Points Status attribute.