Port Function - Edge

This port function is only available on a SCADAPack 47xi device.

Use the Edge port function to create a Linux device for the serial port. An Edge application that opens a connection to the Linux serial port device has exclusive use of that serial port. The port is not available for use for any other RTU platform functions.

When you select the Edge Port Function for a serial port, the following sections and properties are displayed. Configure the properties as required.

Further Information

Specify which points are exposed to the Edge application processor: see Properties that are Common to Configuration Items.

Gateway IP Address (Edge): see Configure Ethernet Ports.

Add and Configure the Entries in an Edge Firewall Table.

For more information about Edge functionality, see the documentation provided with the SCADAPack x70 device.