Configure User Accounts Appropriately

Geo SCADA Expert's security feature can act as an effective security tool, helping to protect your system from being accessed by unauthorized users. But its effectiveness is dependent on the appropriate configuration of user accounts.

To access your system via a user account, a user needs to know the user name and password allocated to that user account. But the protection offered by user accounts does not end there - a user account can be denied access to items and features by its own configuration and the security settings of each database item (in addition to the system-wide security settings made at the server).

For more effective security, you should configure the settings for each user account so that they only provide the required access. Ideally, you should configure a user account so that it only allows the user of that account to access the features and items they need to perform their expected duties. For security purposes, the settings you should pay particular attention to are:

Access Type

Allows you to define whether the user can access Geo SCADA Expert via ViewX, Virtual ViewX, Original WebX, or Pager/SMS (Phone). For more information, see Define whether a User can Access the System via ViewX, Virtual ViewX, Original WebX, or PIN via Application Code.

User Group

Allows you to associate a user account with one or more User Groups. The user account will have its own permissions plus those that are allocated to the User Group(s).

With user accounts that are integrated with Windows or LDAP user accounts, a user's User Group membership is updated automatically at log in (for those Geo SCADA Expert User Groups that are integrated with Windows domain groups or LDAP user groups). For more information, see Associate a Geo SCADA Expert User Group with a Windows Domain Group or LDAP User Group.

Operational

The Operational settings on the ViewX tab—You can use the check boxes to control which operator level features are available to the user.

Configuration

The Configuration settings on the ViewX tab—You can use the check boxes to control which configuration features are available to the user.

Alarm Banner/List

The Alarm Banner/List settings on the ViewX tab—You can use the check boxes to control which alarm features are available to the user.

Explorer Bars

The Explorer Bars settings on the ViewX tab—You can use the check boxes to control which Explorer Bars (navigation hierarchies, such as the Database Bar) are available to the user.

The user-specific security settings that are on the Security tab (only available if the Allow per User option is enabled at the server, and the user accounts are managed directly in Geo SCADA Expert, rather than via the External Authentication feature). You can use the Security settings to define the password length, password strength, password expiry, and so on, for the user account.

External Authentication

On systems on which the External Authentication feature is used, each Geo SCADA Expert user account that is to be managed remotely using Active Directory or LDAP requires a corresponding Windows domain or LDAP user account. When Active Directory is used to manage the user accounts remotely, we recommend that the Windows domain user accounts are given minimal access rights on the Geo SCADA Expert server (see Using External Authentication with Geo SCADA Expert).

Users can log on to ViewX using AVEVA Identity Manager if the PCS Framework is installed and configured (see Geo SCADA Expert Prerequisite Components). You can enable this method of authentication from the Other Authentication Providers section of the External Authentication page (see Using External Authentication with Geo SCADA Expert).

By configuring each user account so that it only has access to the features and items that are relevant to the user of that account, you help to protect your system from:

Remember that on systems on which Geo SCADA Expert is configured to Create users automatically from group membership, you configure the initial settings on the User Pattern Form, rather than the User Form.

External authentication using Windows Active Directory or LDAP extends the capability of Geo SCADA Expert by transferring password and optionally user account management to an external system.

NOTICE

Security threat

On systems on which the 'Everyone' User Group is enabled, all User Accounts on the system automatically inherit the security permissions that are assigned to the 'Everyone' User Group, including the Guest user (which does not require a logon). Each user's security permissions comprise: Everyone permissions + User Group permissions + User Account permissions. To help avoid providing all users with unintended access to features and functionality that should be restricted, use configured User Groups rather than the 'Everyone' User Group. If the 'Everyone' User Group has to be used, it MUST be assigned the minimum permissions required, with access restricted where possible to just the relevant parts of the database. (On new installations, the built-in 'Everyone' User Group is inactive and is not assigned any security permissions by default.)
Failure to follow these instructions can result in equipment damage and a breach in system security.