Last Import Time
Associated with: Sparkplug Publisher Property Translation Tables
You create the content for the Property Translation Table outside of Geo SCADA Expert and then import the file into the database using the Import Property Translation Table pick action. This status attribute indicates when the Import Property Translation Table pick action was last used to successfully import a file into the selected Property Translation Table.
The status attributes displays one of these values:
-
Date and Time—Displays the date and time of last successfully completed request to import a Property Translation Table file into this database item.
If a successful import is followed by an unsuccessful import, the time of the last successful import is displayed.
-
Never imported—The Import Property Translation Table pick action has never been used to import a Property Translation Table file into this particular database item.
ATTENTION: It is possible for a file to be successfully imported, but contain errors. This can happen if the file contains valid information, but some of its entries are not applicable to a Sparkplug Publisher Property Translation Table (see Create the Content for a Property Translation Table). These errors are logged in the Events List for the Property Translation Table database item into which the file is imported.