Troubleshooting a Virtual ViewX Server Installation

This topic provides suggestions to help troubleshoot an installation in which a Virtual ViewX server is not communicating as expected. If an issue still persists after following these guidelines, contact Schneider Electric Support for further help. Be aware that existing warranty and support arrangements determine the level of help that you receive should you need to contact Schneider Electric.

If you recently upgraded to a newer version of Geo SCADA Expert

Check the Release Notes for the new version of Geo SCADA Expert to see if they include advice about upgrading Virtual ViewX.

Also remember that you need to reinstate the settings on your Virtual ViewX Servers if they were previously set to enable users to make configuration changes from Virtual ViewX clients (see Mode of Operation of a Virtual ViewX Server).

Setup for Performance

Adjustments are required if you intend running more than 10 Virtual ViewX clients from a Virtual ViewX server, and either that server or a Geo SCADA Expert server to which it connects is running Geo SCADA Expert 2019. With such a setup, you have to ensure that the client port range is large enough to accommodate at least one advise connection per Virtual ViewX (see Change the Range of Ports for the Client’s Incoming Data in the Geo SCADA Expert Guide to Client Administration).

Setup for Security

We recommend that you ensure that:

  • The address parameters are restricted from the client browser (via the Applications tab on the Virtual UI Server Tool )

  • Anonymous access to Virtual ViewX is disabled (via the Authentication tab on the Virtual UI Server Tool ).

For further information about either of the above, see Working with the Virtual UI Server Tool.

Unexpected Session Terminations

Virtual ViewX uses a 'Disconnected Remote Desktop Session', which means that Virtual ViewX can be terminated if a Registry or Group Policy setting is incorrect. Virtual ViewX manages its sessions, therefore the Windows setting should not be used to apply a time limit.

The registry setting is:

HKEY_LOCAL_MACHINE\Software\Policies\Microsoft\Windows NT\Terminal ServicesMaxDisconnectionTime - this key should not be present.

The Group Policy Setting is:

Remote Desktop Services | Remote Desktop Session Host | Session Time Limits | Set time limit for disconnected sessions - this state should be 'Not Configured'.

Windows 10 and Windows 11 Operating System Support

This section only applies if the Virtual ViewX server is installed on a machine that is running Windows 10 or Windows 11, rather than a server machine that is running on server class hardware (see Operating Systems).

Virtual ViewX uses the Remote Desktop technology within Windows to help create its displays. There are some limitations in the Windows 10 and Windows 11 support of Remote Desktop. These change the behavior of Virtual ViewX when you use a Windows 10 or Windows 11 operating system PC as the Virtual ViewX Server.

On Windows 10 and Windows 11, the Virtual ViewX setup uses the console user as the 'host' for the server. This is implied by the blank account settings on the Sessions tab of the Virtual UI Server Tool (see Working with the Virtual UI Server Tool).

When a user logs in to Virtual ViewX, it is important that a user is logged into the PC console - either by the screen or keyboard locally, or remotely via a remote desktop connection. If no user is logged in, then the Virtual ViewX session may return an error or may display only limited screen content.

Should you wish to create a user manually to remove this restriction, please create a new user, set a password and enter credentials into the Run under this account section of the Sessions tab in the Virtual UI Server Tool (see Working with the Virtual UI Server Tool).

If the PC's name is later changed, the credentials will need changing here and on the Applications tab in the Virtual UI Server Tool. (With the latter, double-click on the Virtual ViewX entry in the table and then select the Credentials tab from the form that gets displayed.)

When such an account is set up, you can use one or more Virtual ViewX sessions without the console user being logged in.

If a console user does log in then current Virtual ViewX sessions are logged out automatically by Windows, but they are permitted to log in again straight away.

Logon Issues

To use a Virtual ViewX client, users have to log on using a valid Geo SCADA Expert User Account. (The Guest User and Super User accounts are not supported by Virtual ViewX.) The User Account has to be provided with the relevant access (see Geo SCADA Expert User Accounts for Accessing Virtual ViewX).

Read this section if you see 'Error 1327' appearing after logon.

The Virtual ViewX server uses two Windows accounts. For more information about these Windows accounts, see User Accounts Created Automatically on the Virtual ViewX Server Machine.

Ports used by the Virtual ViewX Server

Virtual ViewX server installed on a computer that is running a supported Windows Server operating system:

The Virtual ViewX server uses a port internally, set up using the General tab of the Virtual UI Server Tool. We recommend that you choose a Bind to IP setting of 127.0.0.1 to restrict access to the local PC (see Working with the Virtual UI Server Tool).

Please check this setting if you experience issues with the Virtual ViewX server - the port must be set to 6580. This port is dynamically routed to an Internet Information Server port using SSL port 453 by default. You can configure this externally facing port using the IIS Manager application (see Modify your Virtual ViewX Server Installation).

Should you wish users to bypass IIS and use the internal Virtual ViewX port directly, you may simply disable the IIS ports and reconfigure the Bind to IP setting and port number using the Virtual UI Server Tool.

We recommend that you do not enable the HTTP Port when you install Virtual ViewX (see Virtual ViewX Server Setup Wizard). If you initially configure, but later decide to disable, the HTTP port, you should edit the web configuration file to specify that cookies should only be transmitted over a secure channel (see Make Cookies Secure).

Virtual ViewX server installed on a computer that is running Windows 10 or Windows 11:

Virtual ViewX uses a port set up using General tab of the Virtual UI Server Tool (see Working with the Virtual UI Server Tool). You may choose a Bind to IP setting to allow that address to be used by Virtual ViewX clients.

How do I Enable Virtual ViewX Logging?

For information about the Virtual ViewX log files that are created for each instance of Virtual ViewX, see ViewX and Virtual ViewX Logging in the Geo SCADA Expert Guide to Client Administration.

In addition to the above logging, you can also enable logging for the VirtualUI service on the Virtual ViewX server. Please only enable this logging if requested to do so by Schneider Electric Support. For information about how to enable logging for the VirtualUI service, see the Geo SCADA Knowledge Base.