Refreshing a license
Refresh licenses to enable additional features, such as software modules, or additional monitoring devices.
You can refresh licenses online only, directly from the PME server if it has an Internet connection. You use License Configuration Tool to refresh licenses. Offline refresh method is not available.
To refresh a license online:
NOTE: If you have activated license using online method, you can refresh the license using online method only.
- On the PME server, open the License Configuration Tool, and click Refresh License.
The Refresh License page opens.
NOTE: You can access the License Configuration in the install location within
....\Schneider Electric\Power Monitoring Expert\License Configuration Tool
. - On the Refresh License page, click Refresh.
NOTE: By default, the Refresh Method is set to Online.
The licenses are refreshed in the License Configuration Tool.
- Close the License Configuration Tool.
For information on how to configure licensing, see:
- Activating a license
- Returning a license
- Refreshing a license
- Deleting a trial license
- Viewing which licenses have been activated on a system
For reference information see: