Configure Generator and UPS Power Reporting

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

 

To configure the Generator Power Report,

  1. Set up the monitoring devices that record the load data. See Supported Measurements and Devices for details on which measurements are required.
  2. Define the generator power system using the Generator Power Configuration Utility.
  3. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

For information on how to use the report, see Generator Power Report.

 

To configure the UPS Power Report,

  1. Set up the monitoring devices that record the UPS output data. See Supported Measurements and Devices for details on which measurements are required.
  2. Define the UPS power system using the UPS Power Configuration Utility.
  3. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

For information on how to use the report, see UPS Power Report.