Adding a user to a user group

Add a user to a user group to give this user access to the sources and applications assigned to this group in PME.

To add a user to a user group:

  1. In User Manager, select the User Groups tab.
  2. In the user groups table, select the row of the user group to which you want to add users, and then click Edit in this row.
  3. In Edit User Group, select the Users tab, and then, in the user table, select the user you want to add.

    NOTE: Supervisor-level users are not included in the available users list. A supervisor-level user can only be a member of the Global group, not a custom group.

  4. Click Save.

Related topics:

Users

User groups

For information on the Web Application user licenses, see:

For information on related Web Application settings, see:

To customize user access level privileges, see:

For reference information see: