Changing a username

Change a username to give the user a better or more meaningful name.

NOTE: You can only change the name of a standard user in User Manager. You cannot change the name of a Windows user or group.

To change a username:

  1. In User Manager, select the Users tab.
  2. In the users table, select the row of the user for which you want to change the name, and then click Edit in this row.
  3. In Edit Standard User, change the name under Username to the new name, and then click Save.

Related topics:

Users

User groups

For information on the Web Application user licenses, see:

For information on related Web Application settings, see:

To customize user access level privileges, see:

For reference information see: