Library Components
This section provides information on the library components, which are used for monitoring the power system.
The various library components include:
- Circuit Breaker
- Motor
- Switch
- Automatic Transfer Switch
- Lockout/Tagout
- Generator
- Transformer
- Utilities
- Busbar
There are two prevailing standards for electrical equipment:
- ANSI
- IEC
NOTE: The color codes shown in the graphic representations of bind properties for various library components depend on the Advanced One Line (AOL) configuration.