Starting Configuration Manager

To start the Configuration Manager:

  1. Navigate to the ...<Configuration Manager extraction location>\ConfigurationManager folder (typically this folder is on your desktop) and then open ConfigurationManager.exe.

If your system does not meet the Configuration Manager Requirements, functionality will be limited. For example, if you run Configuration Manager on a machine that does not host a power monitoring system, the following message appears:

Next steps:

See Configuration Manager user interface for a description of the controls and options available in the tool.