Connecting or disconnecting a site
Disconnect a site to temporarily remove the devices on this site from the communication network, for example for system testing. Connect a site, that was previously disconnected, to reestablish its communication network connection.
To connect a single site:
- In Device Manager, select the Sites tab.
- In the sites table, select the row of the site you want to connect.
- Right-click in the row and select Connect Site in the context menu.
TIP: Inspect the Communication Status column for the site in the sites table to confirm that the site is connected. Note that there can be a time delay until the communication status is updated in the table.
To connect multiple sites:
- In Device Manager, select the Sites tab.
- In the sites table, select the rows of the sites you want to connect.
TIP: Use
Ctrl+Clickto select individual sites, useShift+clickto select a block of sites. - Right-click in the selected row area and select Connect <number> Sites in the context menu.
TIP: Inspect the Communication Status column for the sites in the sites table to confirm that the sites are connected. Note that there can be a time delay until the communication status is updated in the table.
To disconnect a single site:
- In Device Manager, select the Sites tab.
- In the sites table, select the row of the site you want to disconnect.
- Right-click in the row and select Disconnect Site in the context menu.
TIP: Inspect the Communication Status column for the site in the sites table to confirm that the site is disconnected. Note that there can be a time delay until the communication status is updated in the table.
To disconnect multiple sites:
- In Device Manager, select the Sites tab.
- In the sites table, select the rows of the sites you want to disconnect.
TIP: Use
Ctrl+Clickto select individual sites, useShift+clickto select a block of sites. - Right-click in the selected row area and select Disconnect <number> Sites in the context menu.
TIP: Inspect the Communication Status column for the sites in the sites table to confirm that the sites are disconnected. Note that there can be a time delay until the communication status is updated in the table.
Related topics:
Devices
- Adding a device
- Editing a device
- Deleting a device
- Connecting or disconnecting an Ethernet device
- Enabling or disabling a device
- Viewing a device diagram
Sites
- Adding a site
- Editing a site
- Deleting a site
- Connecting or disconnecting a site
- Enabling or disabling a site
Network
- Exporting network configuration for use in a different system
- Importing network configuration from a different system
For reference information see: