Deleting a site
Delete a site if this site is no longer needed, for example if all the devices connected to the site have been removed from service.
To delete a site:
- In Device Manager, select the Sites tab.
- In the sites table, select the row of the site you want to delete, then right-click in the row and select Delete Site in the context menu. This opens the Delete Site confirmation dialog.
- In the confirmation dialog box, click OK.
To delete multiple sites:
- In Device Manager, select the Sites tab.
- In the sites table, select the rows of the sites you want to delete, then right-click in the selected row area and select Delete <number> Sites in the context menu. This opens the Delete Site confirmation dialog.
TIP: Use
Ctrl+Clickto select individual sites, useShift+clickto select a block of sites. - In the confirmation dialog box, click OK.
Related topics:
Devices
- Adding a device
- Editing a device
- Deleting a device
- Connecting or disconnecting an Ethernet device
- Enabling or disabling a device
- Viewing a device diagram
Sites
- Adding a site
- Editing a site
- Deleting a site
- Connecting or disconnecting a site
- Enabling or disabling a site
Network
- Exporting network configuration for use in a different system
- Importing network configuration from a different system
For reference information see: