Editing a site
Edit a site to update its name or to change its configuration settings. You can edit sites through the Device Manager user interface or through exporting, editing, and then re-importing the site configuration.
To edit a single site through the Device Manager user interface:
- In Device Manager, select the Sites tab.
- In the sites table, select the row of the site you want to edit, then right-click in the row and select Edit Site in the context menu. This opens the Site Configuration dialog.
TIP: You can also double-click a row to open the Site Configuration dialog.
- In Site Configuration, update the configuration settings as needed.
- Click OK.
To edit multiple sites through the Device Manager user interface:
- In Device Manager, select the Sites tab.
- In the sites table, select the rows of the sites you want to edit, then right-click in the selected row area and select Edit <number> Sites in the context menu. This opens the Site Configuration dialog.
TIP: Use
Ctrl+Clickto select individual sites, useShift+clickto select a block of sites. - In Site Configuration, update the configuration settings as needed.
NOTE: Only those settings that are common to all selected sites can be configured at the same time.
- Click OK.
To edit sites through configuration import:
- In Device Manager, select the Sites tab.
- Export the existing configuration in one of the following ways:
- To export the configuration for a single site:
- In the sites table, select the row of the site for which you want to export the configuration, then right-click in the row and select Export Site Configuration for Editing in the context menu. This exports the configuration and saves it in CSV file format to your local Downloads folder.
- To export the configuration for multiple sites:
- In the sites table, select the rows of the sites for which you want to export the configuration, then right-click in the selected row area and select Export Configuration for <number> Sites for Editing in the context menu. This exports the configuration and saves it in CSV file format to your local Downloads folder.
TIP: Use
Ctrl+Clickto select individual sites, useShift+clickto select a block of sites.
- In the sites table, select the rows of the sites for which you want to export the configuration, then right-click in the selected row area and select Export Configuration for <number> Sites for Editing in the context menu. This exports the configuration and saves it in CSV file format to your local Downloads folder.
- To export the configuration for all sites:
- Click Options
in the top right corner of the Sites pane, and then click Export Sites Configuration for Editing in the options menu. This exports the configuration and saves it in CSV file format to your local Downloads folder.
- Click Options
- To export the configuration for a single site:
- Open the exported configuration file in a text editor and edit the configuration information for the sites as needed.
NOTE: Do not edit the content of the UniqueSystemId column.
- Save the file in CSV format.
- In Device Manager, click Import. This opens the import wizard.
- Follow the steps in the import wizard to complete the configuration import.
- Click Finish in the import wizard.
Related topics:
Devices
- Adding a device
- Editing a device
- Deleting a device
- Connecting or disconnecting an Ethernet device
- Enabling or disabling a device
- Viewing a device diagram
Sites
- Adding a site
- Editing a site
- Deleting a site
- Connecting or disconnecting a site
- Enabling or disabling a site
Network
- Exporting network configuration for use in a different system
- Importing network configuration from a different system
For reference information see: