Enabling or disabling a device
Disable a device to remove it from the communication network. For example, disable a device that is out of service. Enable a device that was previously disabled to reconnect it to the communication network.
To enable a single device:
- In Device Manager, select the Devices tab.
- In the devices table, select the row of the device you want to enable.
- Right-click in the row and select Enable Device in the context menu.
TIP: Inspect the Communication Status column for the device in the devices table to confirm that the device is enabled. Note that there can be a time delay until the communication status is updated in the table.
To enable multiple devices:
- In Device Manager, select the Devices tab.
- In the devices table, select the rows of the devices you want to enable.
TIP: Use
Ctrl+Clickto select individual devices, useShift+clickto select a block of devices. - Right-click in the selected row area and select Enable <number> Devices in the context menu.
TIP: Inspect the Communication Status column for the devices in the devices table to confirm that the devices are enabled. Note that there can be a time delay until the communication status is updated in the table.
To disable a single device:
- In Device Manager, select the Devices tab.
- In the devices table, select the row of the device you want to disable.
- Right-click in the row and select Disable Device in the context menu.
TIP: Inspect the Communication Status column for the device in the devices table to confirm that the device is disabled. Note that there can be a time delay until the communication status is updated in the table.
To disable multiple devices:
- In Device Manager, select the Devices tab.
- In the devices table, select the rows of the devices you want to disable.
TIP: Use
Ctrl+Clickto select individual devices, useShift+clickto select a block of devices. - Right-click in the selected row area and select Disable <number> Devices in the context menu.
TIP: Inspect the Communication Status column for the devices in the devices table to confirm that the devices are disabled. Note that there can be a time delay until the communication status is updated in the table.
Related topics:
Devices
- Adding a device
- Editing a device
- Deleting a device
- Connecting or disconnecting an Ethernet device
- Enabling or disabling a device
- Viewing a device diagram
Sites
- Adding a site
- Editing a site
- Deleting a site
- Connecting or disconnecting a site
- Enabling or disabling a site
Network
- Exporting network configuration for use in a different system
- Importing network configuration from a different system
For reference information see: