Changing application access for a user group
Change application access for a user group to add or remove access to certain applications for the members of this group in PME.
To change application access for a user group:
- In User Manager, select the User Groups tab.
- In the user groups table, select the row of the user group for which you want to change application access, and then click Edit
in this row. - In Edit User Group, select the Applications tab, and then select the check boxes for the applications you want to add, or clear the check boxes for the applications you want to remove.
- Click Save.
Related topics:
Users
- Users
- Adding a standard user
- Adding a Windows user
- Adding a Windows group
- Changing a username
- Changing a user password
- Changing a user access level
- Changing user details
- Deleting a user
User groups
- User Groups
- Adding a user group
- Adding a user to a user group
- Adding sources to a user group
- Changing a user group name
- Removing a user from a user group
- Removing sources from a user group
- Changing application access for a user group
- Moving a user between user groups
- Deleting a user group
For information on the Web Application user licenses, see:
For information on related Web Application settings, see:
To customize user access level privileges, see:
For reference information see: