Changing a user password
Change a user password to update the password as part of a security best practice, or because the existing password is lost.
NOTE: You can only change the password for a standard user in User Manager. You cannot change the password for a Windows user.
Strong password criteria: A password must have at least 8 characters and contain at least one character from each of the following:
- uppercase letters
- lowercase letters
- numbers
- special characters.
warning
potential compromise of System availability, integrity, and confidentiality
Use cybersecurity best practices for password creation and management.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Cybersecurity policies that govern user accounts and access - such as least privilege, separation of duties - vary from site to site. Work with the facility IT System Administrator to ensure that user access adheres to the site-specific cybersecurity policies.
To change a user password:
- In User Manager, select the Users tab.
- In the users table, select the row of the user for which you want to change the password, and then click Edit
in this row. - In Edit Standard User, enter the new password under Password and under Confirm Password, and then click Save.
Related topics:
Users
- Users
- Adding a standard user
- Adding a Windows user
- Adding a Windows group
- Changing a username
- Changing a user password
- Changing a user access level
- Changing user details
- Deleting a user
User groups
- User Groups
- Adding a user group
- Adding a user to a user group
- Adding sources to a user group
- Changing a user group name
- Removing a user from a user group
- Removing sources from a user group
- Changing application access for a user group
- Moving a user between user groups
- Deleting a user group
For information on the Web Application user licenses, see:
For information on related Web Application settings, see:
To customize user access level privileges, see:
For reference information see: