Moving a user between user groups

Move a user to a different user group to change which sources and applications this user can access in PME.

To move a user between two user groups, remove the user from the one group and add it to the other group. The order in which these two tasks are performed is not important.

Related topics:

Users

User groups

For information on the Web Application user licenses, see:

For information on related Web Application settings, see:

To customize user access level privileges, see:

For reference information see: