Defining UPS loads

A UPS load represents the logical load attached to a UPS group. This logical load has no functional purpose in the calculations for power redundancy. The UPS load is used only to provide a more complete diagram representation for the UPS system.

To define a UPS load:

  1. Click the UPS load element in the system diagram. The Properties screen appears.

  2. Complete the details for the UPS load:
    1. Load Name: Enter a name for the load.
    2. Description: Enter a description for the load. This field is optional.
  3. Click Done to save the UPS load.

Related Topics: