Defining UPS groups

A UPS group represents a logical grouping of UPS modules. The UPS system contains at least one UPS group and can contain multiple UPS groups. Depending on the UPS system type, the UPS group properties may be different, as shown below. See UPS Power configuration restrictions for more information.

To define a UPS group:

  1. Click on the group object border. The Properties screen appears.

  2. Complete the details for the UPS group:
    1. Group Name: Enter a name for the group. Each UPS group must have a unique name.
    2. Description: Enter a description for the group. This field is optional.
    3. Modules Per Group: Click Add to increase the number of UPS modules in the group. Click Remove to decrease the number. This property is available only for system redundancy types N, N+1 or N+2.
  3. Click Done to save the UPS group.

Related Topics: