Editing a gadget

To edit the settings for a gadget:

  1. Click Settings in the gadget and select Edit to open the Gadget Setup.
  2. In Gadget Setup, change any of the settings on the tabs.

    See Configuring Gadgets for more details.

  3. Click Save to update the gadget settings and to close the Gadget Setup dialog.

TIP: In gadgets where a time range has been specified when the gadgets are configured, the time range selection is included on the gadgets in the dashboard. You can quickly change the time range for the gadget by selecting another period of time from the list in the time range field. The time range is applied to the gadget only while you continue to view the dashboard. If you navigate to another dashboard and then come back to this dashboard, the time range on the gadget reverts to the value that you set when you configured the gadget.

Related topics:

Dashboards:

Gadgets:

For information on how to use Dashboards, see Dashboards.