Moving a dashboard
To move a dashboard:
- In Dashboards, open the Dashboard Library and navigate to the dashboard you want to move.
(Optional) Add a new folder by clicking Add Folderat the bottom of the library panel, or by clicking Add Folder in the Options menu
at the top of the library.
- Right-click the dashboard name or click Options
for this dashboard and select Move To.... This opens the Select Location window.
- In Select Location, select the location where you want to move this dashboard.
- Click OK to move the dashboard.
Related topics:
Dashboards:
- Adding a new dashboard
- Editing a dashboard
- Sharing a dashboard
- Moving a dashboard
- Deleting a dashboard
- Set default options for a dashboard
- Configuring a slideshow
Gadgets:
For reference information see:
For information on how to use Dashboards, see Dashboards.