Copying a report

Copy reports to quickly create new reports that are the same as, or similar to existing reports. For example, create a copy of a report to experiment with the input parameters without affecting the original report. You can also use a copy of a report as a starting point for a new report that shares many of the input settings of the original report.

To copy a report:

  1. In Reports, open the Report Library and navigate to the report you want to copy.
  2. Right-click the report name or click Options for this report and select Duplicate to create a copy in the same folder. Select Copy To to create a copy in a different folder.
  3. (Optional) In the Report Library, select the new report, right-click the report name or click Options for this report and select Edit to open Report Settings. You can also open Report Settings by double-clicking the report name. Change the report Name, Location and access permissions, and the saved Report Inputs to customize the report if necessary.
  4. Save the report.

NOTE: You cannot copy report templates.

Related topics:

Reports:

Subscriptions:

Other

For information on how to use Reports, see Reports.