•   EN
    • DE
    • ES
    • FR
    • IT
    • ZH
  •  
    Show only results that contain ALL words
    Find whole words only
  1. Machine Expert
  2. V1.1
  3. Software
  4. Libraries, Templates and Examples
  5. Libraries
  6. Communication Libraries

Communication Libraries

EMailHandling - Library Guide

This document describes the library which allows your controller to send and receive an email, including attachments, to or from one or several recipients with the possibility to customize the content.

FtpRemoteFileHandling - Library Guide

This document describes the library which offers FTP (File Transfer Protocol) client functionalities to a controller to access and handle files remotely from and to an FTP server.

HttpHandling - Library Guide

With the HttpHandling library, you can implement the HTTP client functionality in your controller application.

Modem - Library Guide

This document describes the modem functions library for EcoStruxure Machine Expert controllers.

MqttHandling - Library Guide

This document describes the library which provides the MQTT client functionality in order to exchange data with other devices over the network through an MQTT message server.

PLCCommunication - Library Guide

This document describes the PLCCommunication library for EcoStruxure Machine Expert controllers.

SE_NetVarUdp - Library Guide

This document describes the library which provides the data exchange between controllers within a network via network variables.

SercosCommunication - Library Guide

This document describes the library which provides tools and application functionality for Sercos III communication.

NOTE: This help is available in English and German.

SnmpManager - Library Guide

This document describes the library which implements a manager for the Internet-standard protocol SNMP (Simple Network Management Protocol). The SNMP manager allows your controller to collect and organize information about managed devices on IP (Internet Protocol) networks and to modify this information in order to change the behavior of the device.

SqlRemoteAccess - Library Guide

This document describes the library which provides SQL (Structured Query Language) client function blocks that allow your controller to connect to an SQL database in order to run SQL queries for reading and writing data.

TcpUdpCommunication - Library Guide

This document describes the library which provides the core functionality for implementing socket-based network communication protocols using TCP (Transmission Control Protocol) client and server, or UDP (User Datagram Protocol) including broadcast and multicast if supported by the platform.

TimeSync - Library Guide

This document describes the library which implements the SNTP (Simple Network Time Protocol) client feature. It allows your controller to connect to an NTP (Network Time Protocol) or SNTP time server in order to synchronize the internal RTC (Real-Time Clock) of the controller in accordance with the primary time standard UTC (Universal Time Coordinated) that is globally unique.

©2020 Schneider Electric. All rights reserved.