Adding users

Prerequisites

notice

LOSS OF ACCESS

  • Record the device username and password in a secure location.

  • Ensure that the password you set is compatible with:

    • The device front panel.

    • Any software used to communicate with the device.

Failure to follow these instructions can result in loss of access to the device and data on the device.

 

To add a user:

  1. Select Device Management > Privacy and Security > Users.
  2. Select Manage Users and then select Add User.
  3. (Optional) Enter a user Description.
  4. Enter and then confirm the Password.
  5. Choose the User Privileges.
  6. Select Save Working Copy.
  7. Synchronize changes.