Password complexity and length settings
This topic describes the configurable parameters for enforcing password complexity and minimum length requirements. The parameters listed here are available across supported devices, though enforcement behavior might vary depending on the device model. For more information, see Product-specific behavior.
Note: Some parameters and options might differ depending on your device model and firmware.
Password complexity and length settings
| Parameter | Values | Description |
|---|---|---|
| Password Complexity | None, IEEE 1686-2013, NERC CIP-007-5 |
Specifies the character diversity enforcement rules for new passwords:
Note: If Password Complexity is set to NERC CIP-007-5 or IEEE 1686-2013, Minimum Password Length must be 6 or greater. |
| Minimum Password Length | 1 to the maximum password length supported by your device | The minimum allowable length for new passwords. |
Product-specific behavior
The password complexity and minimum password length are enforced for all supported devices. However, enforcement behavior might vary depending on the device model.
For the ION8650, password complexity and minimum length are enforced only within PowerLogic™ Engineering Suite. The ION8650 does not support firmware-level enforcement because it lacks the necessary registers to store these values. As a result, password complexity and length rules are not applied directly by the device firmware.
Administrators using the ION8650 should ensure that password policies are consistently applied through software-based user management tools.