Configuring GPS time synchronization
Prerequisites
- Open the device table of contents
- Connect to your device
- Configuring a serial port for GPS time synchronization
To configure GPS time synchronization:
- Select > > .
- Go to Time Synchronization.
- Set the Time Synchronization Type to UTC.
Note: Set Time Synchronization Type to LOCAL if time sync signals are received in local time.
- Set the Time Synchronization Source to COM1 (or COM4).
- Set the Clock Source to COMM.
- Under Use Clock Source Quality Flag, select whether to use or ignore the quality flag.
- Select Save Working Copy.
- Synchronize changes.