Time synchronization settings
Note: The available parameters and values may differ for your device.
Time synchronization settings
| Parameter | Values | Description |
|---|---|---|
| Time Synchronization Type | UTC, LOCAL |
Sets the time format of the time synchronization message:
For NTP, SNTP, and PTP time synchronization, set the Time Synchronization Type to UTC. |
| Time Synchronization Source | COM1, COM4, Ethernet - ION, Ethernet - ION, Ethernet - DNP, Ethernet - PTP, IRIG-B |
Sets which device port accepts time synchronization messages. Time synchronization messages on other ports are ignored. Set the Time Synchronization Source to:
|
| Enable NTP/SNTP Time Synchronization | No, NTP, SNTP |
Sets the time synchronization protocol:
|
| SNTP/NTP Server | Contact your local network administrator for parameter values. | Specifies the IP address (or fully qualified domain name if Domain Name System is active) of the SNTP or NTP server. |
| Time Synchronization Interval | Numeric value or elapsed interval value | Specifies how often the device synchronizes over SNTP. |
| Event Logging Threshold | 0.000001–1.000000 | Specifies the minimum time difference (in seconds) for a time
synchronization to be logged as an event. This parameter can be configured to help prevent the device’s event log from being flooded with time synchronization events. |
| Clock Source | Internal, COMM, Line Freq |
Sets the source for the clock:
|
For more information on the Clock Module, see ION Reference, available on www.se.com.