Configuring NTP or SNTP time synchronization

Prerequisites

To configure NTP/SNTP time synchronization:

  1. Select Basic Setup > Clock > Date and Time.
  2. Go to Time Synchronization.
  3. Set the Time Synchronization Type to UTC.
  4. Set the Time Synchronization Source to Ethernet.
  5. Set Enable NTP/SNTP Time Synchronization to NTP or SNTP, depending on your application.
  6. Enter the SNTP/NTP Server IP address or full host name.

    Recommedation: Use the server host name if available (DNS is enabled); the IP address may change.

  7. (SNTP only) Enter the Time Synchronization Interval.
  8. (NTP only) Enter the Event Logging Threshold.
  9. Set the Clock Source to Internal.
  10. Select Save Working Copy.
  11. Synchronize changes.