Digital input settings
Digital input settings
| Parameter | Values | Description |
|---|---|---|
| Input Mode | Pulse, KYZ, A/C, IRIG-B |
Specifies how the device responds to a digital input signal:
|
| Polarity | Non-inverting, Inverting | Specifies if the signal from the digital port is inverted or not inverted. This setting is ignored if the Input Mode is set to A/C. |
| Debounce | 0.0000–1 | Specifies how long (in seconds) the external signal must remain in a certain state to be considered a valid state change. This helps ignore transient noise states. This setting is ignored if the Input Mode is set to A/C. |
| Port | Port number, Not Used | Your device’s physical digital input port. |
| EventLog Mode | Log Off, Log On | Specifies if events generate log entries. |