Configuring IRIG-B time synchronization

Prerequisites

To configure IRIG-B time synchronization:

  1. Select Basic Setup > Clock > Date and Time.
  2. Go to Time Synchronization.
  3. Set the Time Synchronization Type to UTC.

    Note: Set Time Synchronization Type to LOCAL if time synchronization signals are received in local time.

  4. Set the Time Synchronization Source to IRIG-B.

    Note: This automatically sets the Clock Source to COMM.

  5. Select Save Working Copy.
  6. Synchronize changes.