Configuring a digital output
Prerequisites:
warning
unintended operation
Do not use this device for critical control or protection of persons, animals, property, or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
To configure a digital output:
- Select Basic Setup > Inputs and Outputs > Digital.
- Under Outputs, go to the digital output that you want to configure.
- Enter your Digital output settings.
- Under Actions, select
. - Choose your Digital output link settings.
- Select Apply.
- Select Save Working Copy.
- Synchronize changes.