Digital output link settings
Digital output link settings
| Parameter | Values | Description |
|---|---|---|
| Source | Not Linked, Linked input | When linked, the Boolean value of the Source is sent to the digital output specified by Port. If you leave Source unlinked, the digital output is controlled by Force ON and Force OFF. |
| Force ON | Not Linked, Linked input | This input forces the digital output on when pulsed, regardless of the Source value. The digital output specified by Port is pulsed for one Pulse Width. After pulsing Force ON, Force ON and Force OFF now control the digital output. |
| Force OFF | Not Linked, Linked input | This input forces the specified digital output off when pulsed, regardless of the Source value. The Force OFF input is only valid if the Pulse Width is set to zero. Force OFF is ignored if the Pulse Width is non-zero. After pulsing Force OFF, Force ON and Force OFF now control the digital output. |
| Normal | Not Linked, Linked input | If the digital output is being controlled by Force ON and Force OFF, pulsing Normal changes the digital output control back to Source. |