Embed a Pre-Configured Trend on a Mimic

You can embed pre-configured Trends on your Mimics. Embedded pre-configured Trends update in the same way as Trends that are stored as database items and provide similar advantages to embedded Mimics:

Embedded Trends on Mimics provide a subset of the features that are available on pre-configured Trends. This includes operational-level access to a subset of the menu options on the Trend. Trends that have been configured to display in Inset Windows on Mimics support a slightly different subset of operational-level menu options to Embedded Trends.

To embed a pre-configured Trend on a Mimic:

  1. Display the Mimic that is to contain the embedded Trend. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Select Trend in the Drawing command group on the Graphics Tab.

  3. Draw the outline of the embedded Trend by pressing the left-hand mouse button, and moving the cursor while keeping the left-hand mouse button pressed. The rectangle that is drawn is the space that will be occupied by the embedded Trend.
  4. Release the left-hand mouse button to display a browse window.
  5. Use the browse window to locate the pre-configured Trend that you want to embed.
  6. Select the Trend that is to be embedded, then select the OK button to confirm.
    The browse window is closed and the Trend is embedded.

Alternatively:

  1. Display a Mimic in Design mode (see Displaying a Mimic).
  2. Display the Database Bar (see Display an Explorer Bar).
  3. In the Database Bar, select the pre-configured Trend that you want to embed and drag it onto the Mimic.
    A context sensitive menu is displayed.
  4. Select the Embedded Trend option to embed the Trend on the Mimic.

You can resize the embedded Trend by selecting it and dragging its sides. Similarly, you can reposition it by selecting it and dragging it to a new position.

You can edit the embedded Trend by double-clicking on it (see Editing an Embedded Trend). You can also access editing features by right-clicking on the embedded Trend to display a context sensitive menu (see Mimic Editing Features).