Log On to a Virtual ViewX Client

Geo SCADA Expert provides three distinct options for logging on to a Virtual ViewX client. Each logon option is designed to provide a secure authentication experience to suit your company's preferences and security requisites. A system administrator will be able to advise you as to which option your system and User Account is set up to use. Based on the system configuration and your User Account's setup, you will log on to a Virtual ViewX client using one of the following options:

The single sign-on logon option is only supported from Geo SCADA Expert 2023 onwards. You cannot use 2FA in conjunction with SSO.

User Accounts in Geo SCADA Expert are designed to be allocated to individual members of staff. User Accounts have:

To use a Virtual ViewX client to interact with Geo SCADA Expert, you have to log on via a user account (just like with ViewX clients).

You cannot use the built-in Guest or Super User accounts to log on to a Virtual ViewX client (see Built-in User Accounts).

Further Information

Creating a User Account: see Creating a User Account.

Log off from a Virtual ViewX client: see Log Off from ViewX.

Change Your Password: see Change your Password.

Working with Single and Multiple Databases.