Plan
Use the information provided in this
Use the links in the following table to find the content you are looking for:
Topic | Content |
---|---|
Planning checklist | This is a planning tool to remind you of the different decisions that have be made and actions that have to be taken during the planning process. |
System architecture | Discusses where the system software and the database server can be installed. |
Client types | Introduces the different PME software client types. |
IT Requirements | Provides information on information technology components, such as computer hardware, operating environment, and networking. |
System maintenance | Provides information on database maintenance and recommended actions. |
Disaster recovery strategy | Provides information on disaster recovery and recommended strategy. |
Cybersecurity | Provides recommended actions to help secure your system. |
Licensing | Provides information on software licensing for PME systems. |
System installation and upgrades | Lists considerations related to new system installs and system upgrades. |
Feature selection and design | Provides an overview of the features and modules available in the software. It introduces the different functions, applications and modules and discusses dependencies and design considerations. |
Device Networks | Provides information on the communication links between the software and the monitoring devices. |
System Integration | Provides information on the different approaches and technologies for integrating PME with other systems. |
Deployment considerations | Provides information on the time, effort, and expertise that is required to deploy a PME system. |
Planning references | Links to reference information related to the content of the Planning chapter. |