Licensing configuration

Power Monitoring Expert (PME) is a proprietary software that uses licensing to control its use and distribution. To use PME, you must purchase software licenses and activate them in the system. PME uses a modular licensing structure where different licenses enable different functions in the software. Some of these functions are optional, others are required. The licenses are cumulative, meaning that you can add additional licenses to a system, to enable additional functionality.

notice

LOSS of communication

Activate product and component licenses prior to the expiry of the trial license.
Activate sufficient licenses for the servers and devices in your system.
Export the existing hierarchy template out of Power Monitoring Expert before importing a new template. The new template can overwrite the existing template, which can permanently remove all information contained in the original.
Backup or archive any SQL Server database data before adjusting any database memory options.
Only personnel with advanced knowledge of SQL Server databases should make database parameter changes.

Failure to follow these instructions can result in loss of data.

 

For information on how to configure licensing, see:

For reference information see: